ZHCSIF5F December 2015 – April 2019 TPS99000-Q1
PRODUCTION DATA.
The current limit of the LM3409 is determined by the current draw of the IADJ pin of the TPS99000-Q1, which is controlled by an internal DAC and an external resistor connected to the R_IADJ pin of the TPS99000-Q1. The approximate peak current limit can be calculated by the following equation:
Where: