ZHCSLZ6 September 2020 TPS65982DMC
PRODUCTION DATA
The TPS65982DMC Adapter Input Power is the main power input to the system. When placing/routing the external power path it is important to consider the current handling. It is recommended placing a TVS such as the TVS2200 close to the Adapter Input Power Jack, to absorb any inductive ringing from a hot plug. The TPS65982DMC external power path should be placed in the same area as the Adapter Input Power Jack. The HV_GATE1/2 pins are high voltage nets, so it is recommended to space them from sensitive signals. The HV_GATE1/2 nets can be route through vias if needed. The SENSE_P/N current sense measures the current flowing into the system and the routing should be as direct, minimal layer changes, and kept from switching nets/signals.