ZHCSO18A december 2022 – june 2023 TPS281C30
PRODUCTION DATA
Capacitive Charging Circuit shows the typical set up for a capacitive load application and the internal blocks that function when the device is used. Note that all capacitive loads will have an associated "load" in parallel with the capacitor that is described as a resistive load but in reality it can be inductive or resistive.
The first thing to check is that the nominal DC current, INOM, is acceptable for the TPS281C30 device. This can easily be done by taking the RθJA from the Thermal Section and multiplying the RON of the TPS281C30 and the INOM with it, add the ambient temperature and if that value is below the thermal shutdown value the device can operate with that load current. For an example of this calculation see the Applications Section.
The second key care about for this application is to make sure that the capacitive load can be charged up completely without the device hitting thermal shutdown. This is because if the device hits thermal shutdown during the charging, the resistive nature of the load in parallel with the capacitor will start to discharge the capacitor over the duration the TPS281C30x is off. Note that there are some application with high enough load impedance that the TPS281C30 hitting thermal shutdown and trying again is acceptable; however, for the majority of applications the system should be designed so that the TPS281C30x does not hit thermal shutdown while charging the capacitor.
With the current clamping feature of the TPS281C30x, capacitors can be charged up at a lower inrush current than other high current limit switches. This lower inrush current means that the capacitor will take a little longer to charge all the way up. However, to minimize this longer charge time during startup, TPS281C30 implements an inrush current handling feature described in On-State Short Circuit Behavior. When the EN pin goes high to turn on the high side switch, the device will default its current limit threshold to ILIM_STARTUP for a duration of ILIM_STARTUP_DELAY. During this delay period, a capacitive load can be charged at a higher rate than what typical ICL would allow and FAULT will be masked to prevent unwanted Fault triggers. After ILIM_STARTUP_DELAY, the current limit will default back to ICL and Fault will work normally.
The initial inrush current period when the current limit is higher enables two different system advantages when driving loads:
While in current limiting mode, at any level, the device will have a high power dissipation. If the FET temperature exceeds the over-temperature shutdown threshold, the device will turn off just the channel that is overloaded. After cooling down, the device will re-try. If the device is turning off prematurely on start-up, it is recommended to improve the PCB thermal layout, lower the current limit to lower power dissipation, or decrease the inrush current (capacitive loading). t limit to lower power dissipation, or decrease the inrush current (capacitive loading).
For more information about capacitive charging with high side switches see the How to Drive Capacitive Loads application note. This application note has information about the thermal modeling available along with quick ways to estimate if a high side switch will be able to charge a capacitor to a given voltage.