SLVSC11C June 2013 – December 2014 TPS2592AA , TPS2592AL
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPA2592xx is a smart eFuse. It is typically used for Hot-Swap and Power rail protection applications. It operates from 4.5 V to 18 V with programmable current limit and undervoltage protection. The device aids in controlling the in-rush current and provides precise current limiting during overload conditions for systems such as Set-Top-Box, DTVs, Gaming Consoles, SSDs/HDDs and Smart Meters. The device also provides robust protection for multiple faults on the sub-system rail.
The following design procedure can be used to select component values for the device. Alternatively, the WEBENCH® software may be used to generate a complete design. The WEBENCH® software uses an iterative design procedure and accesses a comprehensive database of components when generating a design. Additionally, a spreadsheet design tool TPS2592 Design Calculator (SLUC571) is available on web folder. This section presents a simplified discussion of the design process.
Figure 36. Typical Application Schematic: Simple 3.7-A e-Fuse for STBs
| DESIGN PARAMETER | EXAMPLE VALUE |
|---|---|
| Input voltage range, VIN | 12 V |
| Undervoltage lockout set point, V(UV) | Default: VUVR = 4.3 V |
| Overvoltage protection set point , V(OV) | Default: VOVC = 15 V |
| Load at Start-Up , RL(SU) | 4 Ω |
| Current limit, IOL = IILIM | 3.7 A |
| Load capacitance , COUT | 1 µF |
| Maximum ambient temperatures , TA | 85°C |
The following design procedure can be used to select component values for the TPS2592x.
This design procedure below seeks to control the junction temperature of device under both static and transient conditions by proper selection of output ramp-up time and associated support components. The designer can adjust this procedure to fit the application and design criteria.
The RILIM resistor at the ILIM pin sets the over load current limit, this can be set using Equation 4.
For IOL= IILIM = 3.7 A, from equation 4, RILIM = 100 kΩ, choose closest standard value resistor with 1% tolerance.
The undervoltage lockout (UVLO) trip point is adjusted using the external voltage divider network of R1 and R2 as connected between IN, EN/UVLO and GND pins of the device. The values required for setting the undervoltage are calculated solving Equation 5.
Where VENR = 1.4 V is enable voltage rising threshold.
Since R1 and R2 will leak the current from input supply (VIN), these resistors should be selected based on the acceptable leakage current from input power supply (VIN). The current drawnby R1 and R2 from the power supply {IR12 = VIN/(R1 + R2)}.
However, leakage currents due to external active components connected to the resistor string can add error to these calculations. So, the resistor string current, IR12 must be chosen to be 20x greater than the leakage current expected.
For default UVLO of VUVR = 4.3 V, select R2 = OPEN, and R1 = 1 MΩ. Since EN/UVLO pin is rated only to 7 V, it cannot be connected directly to VIN= 12 V. It has to be connected through R1 = 1 MΩ only, so that the pull-up current for EN/UVLO pin is limited to < 20 µA.
The power failure threshold is detected on the falling edge of supply. This threshold voltage is 4% lower than the rising threshold, VUVR. This is calculated using Equation 6.
Where VUVR is 4.3V, Power fail threshold set is : 4.1 V
For a successful design, the junction temperature of device should be kept below the absolute-maximum rating during both dynamic (start-up) and steady state conditions. Dynamic power stresses often are an order of magnitude greater than the static stresses, so it is important to determine the right start-up time and in-rush current limit required with system capacitance to avoid thermal shutdown during start-up with and without load.
The ramp-up capacitor CdVdT needed is calculated considering the two possible cases:
During start-up, as the output capacitor charges, the voltage difference as well as the power dissipated across the internal FET decreases. The average power dissipated in the device during start-up is calculated using Equation 8.
For TPS2592xx, the inrush current is determined as,
Power dissipation during start-up is:
Equation 8 assumes that load does not draw any current until the output voltage has reached its final value.
When load draws current during the turn-on sequence, there will be additional power dissipated. Considering a resistive load during start-up (RL(SU)), load current ramps up proportionally with increase in output voltage during TdVdT time. The average power dissipation in the internal FET during charging time due to resistive load is given by:
Total power dissipated in the device during startup is:
Total current during startup is given by:
If I(STARTUP) > IOL, the device limits the current to IOL and the current limited charging time is determined by:
The power dissipation, with and without load, for selected start-up time should not exceed the shutdown limits as shown in Figure 37.
For the design example under discussion, select ramp-up capacitor CdVdT = OPEN. Then, using Equation 2.
The inrush current drawn by the load capacitance (COUT) during ramp-up using Equation 7.
The inrush Power dissipation is calculated, using Equation 8.
For 90 mW of power loss, the thermal shut down time of the device should not be less than the ramp-up time TdVdT to avoid the false trip at maximum operating temperature. From thermal shutdown limit graph Figure 37 at
TA = 85°C, for 90 mW of power, the shutdown time is infinite. So it is safe to use 0.79 ms as start-up time without any load on output.
Considering the start-up with load 4 Ω, the additional power dissipation, when load is present during start up is calculated, using Equation 9.
The total device power dissipation during start up, using Equation 10 is:
From thermal shutdown limit graph at TA = 85°C, the thermal shutdown time for 6.09 W is more than 100 ms. So it is well within acceptable limits to use no external capacitor (CdV/dT) with start-up load of 4 Ω.
If, due to large COUT, there is a need to decrease the power loss during start-up, it can be done with increase of CdVdT capacitor.
CVIN is a bypass capacitor to help control transient voltages, unit emissions, and local supply noise. Where acceptable, a value in the range of 0.001 μF to 0.1 μF is recommended for CVIN.
Figure 40. Inrush and Reverse Current Protection for Hold-Up Capacitor Application (e.g., SSD) | DESIGN PARAMETER | EXAMPLE VALUE |
|---|---|
| Input voltage range, VIN | 12 V |
| Undervoltage lockout set point, V(UV) | 10.8 V |
| Overvoltage protection set point , V(OV) | Default: VOVC = 15 V |
| Load at Start-Up , RL(SU) | 1000 Ω |
| Current limit, IOL= IILIM | 3 A |
| Load capacitance , COUT | 4700 µF |
| Maximum ambient temperatures , TA | 85°C |
The RILIM resistor at the ILIM pin sets the over load current limit, this can be set using Equation 4.
For IOL = IILIM = 3 A, from equation 4, RILIM = 76.8 kΩ. Choose closest standard value resistor with 1% tolerance.
The undervoltage lockout (UVLO) trip point is adjusted using the external voltage divider network of R1 and R2 as connected between IN, EN/UVLO and GND pins of the device. The values required for setting the undervoltage are calculated solving Equation 5.
For UVLO of V(UV) = 10.8 V, select R2 = 150 kΩ, and R1 = 1 MΩ.
The power failure threshold is detected on the falling edge of supply. This threshold voltage is 4% lower than the rising threshold, V(UV). This is calculated using Equation 6.
Where V(UV) = 10.73 V, Power fail threshold set is : V(PFAIL) = 10.35 V
For a successful design, the junction temperature of device should be kept below the absolute-maximum rating during both dynamic (start-up) and steady state conditions. Dynamic power stresses often are an order of magnitude greater than the static stresses, so it is important to determine the right start-up time and in-rush current limit required with system capacitance to avoid thermal shutdown during start-up with and without load.
For the design example under discussion, select ramp-up capacitor CdVdT = 22 nF. Then, using Equation 2.
The inrush current drawn by the load capacitance (COUT) during ramp-up using Equation 7.
The inrush Power dissipation is calculated, using Equation 8.
Considering the start-up with load 1000 Ω, the additional power dissipation, when load is present during start up is calculated, using Equation 9.
The total device power dissipation during start up is:
From thermal shutdown limit graph at TA = 85°C, the thermal shutdown time for 1.3 W is more than 300 ms. So the device will start safely.
If CdVdT = 4.7 nF was used, the device would have tried to charge the 4700 uF output cap with inrush current of 986 mA in 57.24 ms, dissipating power of 5.94 W. This is outside the safe starting condition of the device, and would have led the device to enter thermal shutdown during start-up.
To prevent damage to the TPS2592x, it is necessary to keep internal power dissipation (PD) below the levels specified in below Table. The power dissipation is defined as (PD = (VIN – VOUT) x IOUT).
| MIN | MAX | UNIT | ||
|---|---|---|---|---|
| Maximum Power Dissipation | –40°C ≤ TA ≤ +85°C | 40 | W | |
| 0°C ≤ TA ≤ +85°C | 50 | |||
During normal operation PD is low ( typically < ½ Watt) because the FET is fully on with low (VIN – VOUT). However, during short circuit and surge protection the FET may be only partially on and (VIN – VOUT) can be high.
Example 1: Short Circuit on Output → VIN = 12 V, ILIMIT = 3 A. TJ = –40°C
Example 2: Short Circuit on Output → VIN = 13.2 V, ILIMIT = 3.7 A
Example 3: Surge Clamp VIN = 12 V, ILIMIT = 3 A. TJ = 0°C, VSURGE =19 V, VCLAMP = 15 V