ZHCSHL4I October 2008 – December 2017
PRODUCTION DATA.
请参考 PDF 数据表获取器件具体的封装图。
The TPS23754 has a number of internal comparators with hysteresis for stable switching between the various states. Figure 21 relates the parameters in the Electrical Characteristics to the PoE states. The mode labeled idle between classification and operation implies that the DEN, CLS, and RTN pins are all high impedance. The state labeled Mark, which is drawn in dashed lines, is part of the new type 2 hardware class state machine.
Figure 21. Threshold Voltages