4 Revision History
Changes from Revision D (January 2023) to Revision E (March 2023)
- Deleted text from the first paragraph of
Go
Changes from Revision C (April 2022) to Revision D (January 2023)
- 向封装信息表中添加了 TCAN1043AT-Q1。Go
- Added part number TCAN1043AT-Q1 to the data sheet
Specifications
Go
- Added minimum specification to the tSILENCE parameter in the Device Characteristics sectionGo
- Changed Figure 7-6 to remove the nSTB signal from the TX block.Go
- Added a link to Table 8-1 in the nFAULT Pin sectionGo
- Changed Table 8-1 to add a comment in the Power-up, Wake-up Source Recognition and TXDRXD event
flags in the Internal and External Fault Indicators
sectionGo
- Changed Figure 8-4 to
accurately reflect the behavior of the SWE timer. Added notes 4 and 5 showing
the transition from silent mode to sleep mode due to SWE timer
timeout.Go
- Added Figure 8-5 to explain the steps to transition from sleep mode to silent
or normal mode when sleep mode is entered due to SWE timer
timeout.Go
- Added a paragraph describing the steps needed to enter Normal or Silent
mode directly from Sleep mode using EN and nSTB pins in the section. Go
- Changed Figure 8-8 to indicate tINH_SLP_STB delay on the INH
waveformGo
- Changed Figure 8-9
to indicate tINH_SLP_STB delay on the INH waveformGo
- Changed Figure 8-10 to convert '&' to 'and', clarified that RXD pin is in High Impedance
in the 'CAN Off state'Go
- Added Note 2 to Figure 8-10
Go
- Changed text From: "The CAN Transceiver blocks its transmitter and
receiver" To: "The CAN transceiver blocks its transmitter" in the CAN
Active sectionGo
Changes from Revision B (December 2021) to Revision C (April 2022)
- 删除了封装信息表中 SOT (DYY) 封装的产品预发布。Go
- Changed the INH pin transistor connection in Figure 8-1
Go
Changes from Revision A (October 2021) to Revision B (December 2021)
- 删除了封装信息表中 SOIC (D) 封装的产品预发布。Go
Changes from Revision * (January 2021) to Revision A (October 2021)