ZHCSP69E August 2009 – May 2022 TCA9535
PRODUCTION DATA
In the event of a glitch or data corruption, TCA9535 can be reset to its default conditions by using the power-on reset feature. Power-on reset requires that the device go through a power cycle to be completely reset. This reset also happens when the device is powered on for the first time in an application.
The two types of power-on reset are shown in Figure 9-1 and Figure 9-2.
Figure 9-1 VCC Is Lowered Below 0.2 V Or 0 V And Then Ramped Up To
VCC
Figure 9-2 VCC Is Lowered Below The Por Threshold, Then Ramped Back Up To
VCCTable 9-1 specifies the performance of the power-on reset feature for TCA9535 for both types of power-on reset.
| PARAMETER(1) | MIN | TYP | MAX | UNIT | ||
|---|---|---|---|---|---|---|
| VCC_FT | Fall rate | See Figure 9-1 | 0.1 | ms | ||
| VCC_RT | Rise rate | See Figure 9-1 | 0.01 | ms | ||
| VCC_TRR | Time to re-ramp (when VCC drops to VVOR_MIN – 50 mV or when VCC drops to GND) | See Figure 9-1 | 1 | µs | ||
| VCC_GH | The level (referenced to VCC) that VCC can glitch down to, but not cause a functional disruption when VCC_GW | See Figure 9-3 | 1.2 | V | ||
| VCC_MV |
The minimum voltage that VCC can glitch down to without causing a reset (VCC_GH must not be violated) |
See Figure 9-3 | 1.5 | V | ||
| VCC_GW | Glitch width that will not cause a functional disruption | See Figure 9-3 | 10 | μs | ||
| VPORF | Voltage trip point of POR on falling VCC | 0.75 | 1 | 1 | V | |
| VPORR | Voltage trip point of POR on rising VCC | 1.2 | 1.5 | V | ||
Glitches in the power supply can also affect the power-on reset performance of this device. The glitch width (VCC_GW) and height (VCC_GH) are dependent on each other. The bypass capacitance, source impedance, and device impedance are factors that affect power-on reset performance. Figure 9-3 and Table 9-1 provide more information on how to measure these specifications.
Figure 9-3 Glitch
Width And Glitch HeightVPORR is critical to the power-on reset. VPORR is the voltage level at which the reset condition is released and all the registers and the I2C/SMBus state machine are initialized to their default states. The value of VPOR differs based on the VCC being lowered to or from 0. Figure 9-4 and Table 9-1 provide more details on this specification.
Figure 9-4 VPOR