SNAS624B March   2014  – May 2015 LMX2492 , LMX2492-Q1

PRODUCTION DATA.  

  1. 1 Features
  2. 2  Applications
  3. 3 Description
  4. 4 Simplified Schematic
  5. 5 Revision History
  6. 6 Pin Configuration and Functions
  7. 7 Specifications
    1. 7.1 Absolute Maximum Ratings
    2. 7.2 Storage Conditions
    3. 7.3 ESD Ratings
    4. 7.4 Recommended Operating Conditions
    5. 7.5 Thermal Information
    6. 7.6 Electrical Characteristics
    7. 7.7 Timing Requirements, Programming Interface (CLK, DATA, LE)
    8. 7.8 Typical Characteristics
  8. 8 Detailed Description
    1. 8.1  Overview
    2. 8.2  Functional Block Diagram
    3. 8.3  Feature Description
      1. 8.3.1  OSCin Input
      2. 8.3.2  OSCin Doubler
      3. 8.3.3  R Divider
      4. 8.3.4  PLL N Divider
      5. 8.3.5  Fractional Circuitry
      6. 8.3.6  PLL Phase Detector and Charge Pump
      7. 8.3.7  External Loop Filter
      8. 8.3.8  Fastlock and Cycle Slip Reduction
      9. 8.3.9  Lock Detect and Charge Pump Voltage Monitor
        1. 8.3.9.1 Charge Pump Voltage Monitor
        2. 8.3.9.2 Digital Lock Detect
      10. 8.3.10 FSK/PSK Modulation
      11. 8.3.11 Ramping Functions
        1. 8.3.11.1 Ramp Count
        2. 8.3.11.2 Ramp Comparators and Ramp Limits
      12. 8.3.12 Power on Reset (POR)
    4. 8.4  Device Functional Modes
      1. 8.4.1 Continuous Frequency Generator
        1. 8.4.1.1 Integer Mode Operation
        2. 8.4.1.2 Fractional Mode Operation
      2. 8.4.2 Modulated Waveform Generator
    5. 8.5  Programming
      1. 8.5.1 Loading Registers
    6. 8.6  Register Map
    7. 8.7  Register Field Descriptions
      1. 8.7.1 POWERDOWN and Reset Fields
      2. 8.7.2 Dividers and Fractional Controls
        1. 8.7.2.1 Speed Up Controls (Cycle Slip Reduction and Fastlock)
    8. 8.8  Lock Detect and Charge Pump Monitoring
    9. 8.9  TRIG1,TRIG2,MOD, and MUXout Pins
    10. 8.10 Ramping Functions
    11. 8.11 Individual Ramp Controls
  9. 9 Applications and Implementation
    1. 9.1 Application Information
    2. 9.2 Typical Applications
      1. 9.2.1 Design Requirements
      2. 9.2.2 Detailed Design Procedure
      3. 9.2.3 Application Performance Plot - Sawtooth Waveform Example
      4. 9.2.4 Application Performance Plot - Flat Top Triangle Waveform
      5. 9.2.5 Applications Performance Plot -- Complex Triggered Ramp
  10. 10Power Supply Recommendations
  11. 11Layout
    1. 11.1 Layout Guidelines
    2. 11.2 Layout Example
  12. 12Device and Documentation Support
    1. 12.1 Device Support
      1. 12.1.1 Development Support
    2. 12.2 Documentation Support
      1. 12.2.1 Related Documentation
    3. 12.3 Related Links
    4. 12.4 Community Resources
    5. 12.5 Trademarks
    6. 12.6 Electrostatic Discharge Caution
    7. 12.7 Glossary
  13. 13Mechanical, Packaging, and Orderable Information

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

9 Applications and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

9.1 Application Information

The LMX2492/92-Q1 can be used in a broad class of applications such as generating a single frequency for a high frequency clock, generating a tunable range of frequencies, or generating swept waveforms that can be used in applications such as radar.

9.2 Typical Applications

The following schematic is an example of hat could be used in a typical application.

LMX2492 LMX2492-Q1 sch_apps_snas624.gif

9.2.1 Design Requirements

For these examples, it will be assumed that there is a 100 MHz input signal and the output frequency is between 9400 and 9800 MHz with various modulated waveforms.

Parameter Symbol Value Comments
Input Frequency OSCin 100 MHz
Phase Detector Frequency Fpd 100 MHz There are many possibilities, but this choice gives good performance and saves a little current (as shown in the electrical specifications).
VCO Frequency Fvco 9400 - 9800 MHz (Simple Chirp) In the different examples, the VCO frequency is actually changing. However, the same loop filter design can be used for all three.
9400 - 9800 (Flattened Ramp)
9500 - 9625 MHz (Complex Triggered Ramp
VCO Gain Kvco 200 MHz/V This parameter has nothing to do with the LMX2492/92-Q1, but is rather set by the external VCO choice.

9.2.2 Detailed Design Procedure

The first step is to calculate the reference divider (PLL_R) and feedback divider (PLL_N) values as shown in the table that follows.

Parameter Symbol and Calculations Value Comments
Average
VCO Frequency
FvcoAvg
= (FvcoMax + FvcoMin)/2
9600 MHz To design a loop filter, one designs for a fixed VCO value, although it is understood that the VCO will tune around. This typical value is usually chosen as the average VCO frequency.
VCO Gain Kvco 200 MHz/V This parameter has nothing to do with the LMX2492/92-Q1, but is rather set by the external VCO choice. In this case, it was the RFMD1843 VCO.
PLL Loop Bandwidth BW 380 kHz This bandwidth is very wide to allow the VCO frequency to be modulated.
Charge Pump Gain CPG 3.1 mA Using the larger gain allows a wider loop bandwidth and gives good phase performance.
R Divider PLL_R
= OSCin / Fpd
1 This value is calculated from previous values.
N Divider PLL_N
= Fvco / Fpd
96 This value is calculated from previous values.
Loop Filter Components C1_LF 68 pF These were calculated by TI design tools.
C2_LF 3.9 nF
C3_LF 150 pF
R2_LF 390 ohm
R3_LF 390 ohm

Once a loop filter bandwidth is chosen, the external loop filter components of C1_LF, C2_LF, C3_LF, R2_LF, and R3_LF can be calculated with a tool such as the Clock Architect tool available at www.ti.com. It is also highly recommended to look at the EVM instructions. The CodeLoader software is an excellent starting point and example to see how to program this device.

9.2.3 Application Performance Plot - Sawtooth Waveform Example

Using the above design, it can be programmed to generate a sawtooth waveform with the following paramters.

Parameter Symbol Value
Ramp Duration ΔT 100 uS
VCO Frequency Fvco 9400 - 9800 MHz
Range ΔF 9400 - 9800 MHz = 400 MHz Change
LMX2492 LMX2492-Q1 example_ramp01_nas624.gif

Because we want the ramp length to be 100 us, this works out to 10,000 phase detector cycles which means that RAMP0_LEN=10000. To change 400 MHz, we know that each one of the 10000 steps is 40 kHz. Given the fractional denominator is 224 = 16777216 and the phase detector frequency is 100 MHz, this implies that the fractional numerator at the end of the ramp will be 6711. However, since this 6711 number is not exact (closer to 6718.8864), the ramp will creep if we do not reset it. Therefore, we set reset the ramp. After the ramp finishes, we want to start with the same ramp, so RAMP0_NEXT is RAMP0. The results of this analysis are in the table below:

RAMP RAMP0_LEN RAMP0_INC RAMP0_NEXT RAMP0_RST
RAMP0 ΔT × Fpd = 100 us / 100 MHz
= 10000
(ΔF / Fpd) /RAMP0_LEN × 224
= (400/100)/10000 ×16777216 = 6711
0 1

The actual measured waveform for this is shown in the following figure. Note that the frequency that was actually measured was from the divide by two output of the VCO and therefore the measured frequency was half of the actual frequency presented to the PLL. This ramping waveform does show some undershoot as the frequency rapidly returns from 9800 MHz ( 4900 MHz on the plot) to 9400 MHz (4700 MHz on the plot). This undershoot can be mitigated by adding additional ramps.

LMX2492 LMX2492-Q1 ai_ramp_sawtooth.png

9.2.4 Application Performance Plot - Flat Top Triangle Waveform

Now consider pattern as shown below. The ramp is sometimes used because it can better account for Doppler Shift. The purpose for making the top and bottom portions flat is to help reduce the impact of the PLL overshooting and undershooting in order to make the sloped ramped portions more linear.

Parameter Symbol Value
Ramp Duration ΔT0 10 uS
ΔT1 90 uS
ΔT2 10 uS
ΔT3 90 uS
Range ΔF0 0
ΔF1 400 MHz
ΔF2 0
ΔF3 -400 MHz
LMX2492 LMX2492-Q1 example_ramp02_nas624.gif
RAMP RAMPx_LEN RAMPx_INC RAMPx_NEXT RAMPx_RST
RAMP0 10 us/ 100 MHz
=1000
0 1 1
RAMP1 90 us / 100 MHz
=9000
(ΔF / Fpd) /RAMP1_LEN × 224
= (400/100)/9000 ×16777216 = 7457
2 0
RAMP2 10 us/ 100 MHz
=1000
0 3 0
RAMP3 90 us / 100 MHz
=9000
(ΔF / Fpd) /RAMP1_LEN × 224
= (-400/100)/9000 ×16777216 = -7457
Program in 2's complement of -7457
= 230-7457 = 1073734367
0 0

The actual measured waveform for this is shown in the following figure. Note that the frequency that was actually measured was from the divide by two output of the VCO and therefore the measured frequency was half of the actual frequency presented to the PLL. The flattened top and bottom of this triangle wave help mitigate the overshoot and undersoot in the frequency.

LMX2492 LMX2492-Q1 ai_ramp_triangle.png

The actual measured waveform for this is shown in the following figure. Note that the frequency that was actually measured was from the divide by two output of the VCO and therefore the measured frequency was half of the actual frequency presented to the PLL. The flattened top and bottom of this triangle wave help mitigate the overshoot and undersoot in the frequency.

9.2.5 Applications Performance Plot -- Complex Triggered Ramp

In this example, the modulation is not started until a trigger pulse from the MOD terminal goes high. Assume a phase detector frequency of 100 MHz and we RAMP1 to be 60 us and ramps 2,3,and 4 to be 12 us each. We set the next trigger for RAMP0 to be trigger A and define trigger A to be the MOD terminal. Then we configure as follows:

LMX2492 LMX2492-Q1 ex_ramp3_snas624.gifFigure 6. Complex Triggered Ramp Example
RAMP RAMPx
_LEN
RAMPx_
INC
RAMPx_FL RAMPx
_NEXT
RAMPx_FLAG RAMPx_
NEXT_TRIG
RAMPx_RST
RAMP0 1 0 0 1 FLAG0 and FLAG1 TRIG A 1
RAMP1 6000 1073730639 0 2 FLAG0 and FLAG1 TOC Timeout 1
RAMP2 1200 27963 1 3 Disabled TOC Timeout 0
RAMP3 1200 17476 0 4 FLAG1 TOC Timeout 0
RAMP4 1200 10486 0 1 FLAG0 and FLAG1 TOC Timeout 0

The actual measured waveform for this is shown in the following figure. Note that the frequency that was actually measured was from the divide by two output of the VCO and therefore the measured frequency was half of the actual frequency presented to the PLL. The flattened top and bottom of this triangle wave help mitigate the overshoot and undersoot in the frequency.

LMX2492 LMX2492-Q1 ai_ramp_complextriggered.pngFigure 7. Actual Measurement for Complex Triggered Ramp