SNOSBH0D May 2000 – November 2015 LF156 , LF256 , LF356
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
These are op amps with JFET input devices. These JFETs have large reverse breakdown voltages from gate to source and drain eliminating the need for clamps across the inputs. Therefore large differential input voltages can easily be accommodated without a large increase in input current. The maximum differential input voltage is independent of the supply voltages. However, neither of the input voltages should be allowed to exceed the negative supply as this will cause large currents to flow which can result in a destroyed unit.
Exceeding the negative common-mode limit on either input will force the output to a high state, potentially causing a reversal of phase to the output. Exceeding the negative common-mode limit on both inputs will force the amplifier output to a high state. In neither case does a latch occur since raising the input back within the common-mode range again puts the input stage and thus the amplifier in a normal operating mode.
Exceeding the positive common-mode limit on a single input will not change the phase of the output however, if both inputs exceed the limit, the output of the amplifier will be forced to a high state.
These amplifiers will operate with the common-mode input voltage equal to the positive supply. In fact, the common-mode voltage can exceed the positive supply by approximately 100 mV independent of supply voltage and over the full operating temperature range. The positive supply can therefore be used as a reference on an input as, for example, in a supply current monitor and/or limiter.
Precautions should be taken to ensure that the power supply for the integrated circuit never becomes reversed in polarity or that the unit is not inadvertently installed backwards in a socket as an unlimited current surge through the resulting forward diode within the IC could cause fusing of the internal conductors and result in a destroyed unit.
All of the bias currents in these amplifiers are set by FET current sources. The drain currents for the amplifiers are therefore essentially independent of supply voltage.
As with most amplifiers, care should be taken with lead dress, component placement and supply decoupling in order to ensure stability. For example, resistors from the output to an input should be placed with the body close to the input to minimize pick-up and maximize the frequency of the feedback pole by minimizing the capacitance from the input to ground.
A feedback pole is created when the feedback around any amplifier is resistive. The parallel resistance and capacitance from the input of the device (usually the inverting input) to AC ground set the frequency of the pole. In many instances the frequency of this pole is much greater than the expected 3-dB frequency of the closed loop gain and consequently there is negligible effect on stability margin. However, if the feedback pole is less than approximately six times the expected 3-dB frequency a lead capacitor should be placed from the output to the input of the op amp. The value of the added capacitor should be such that the RC time constant of this capacitor and the resistance it parallels is greater than or equal to the original feedback pole time constant.
Figure 35. Settling Time Test Circuit
Settling time is tested with the LF35x connected as unity gain inverter and LF357 connected for AV = −5
Connect the circuit components as shown in Figure 35. In particular, use FET to isolate the probe capacitance.
Apply a 10-V step function to the input.
Use an oscilloscope to probe the circuit as shown in Figure 35.
Large Signal Inverter Output, VOUT (from Settling Time Circuit)
Figure 36. LF355
Figure 38. LF357
Figure 39. Low Drift Adjustable Voltage Reference
Figure 40. Fast Logarithmic Converter

Figure 41. Precision Current Monitor
Figure 42. 8-Bit D/A Converter With Symmetrical Offset Binary Operation
| EO | B1 | B2 | B3 | B4 | B5 | B6 | B7 | B8 | COMMENTS |
|---|---|---|---|---|---|---|---|---|---|
| +9.920 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | Positive Full-Scale |
| +0.040 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | (+) Zero-Scale |
| −0.040 | 0 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | (−) Zero-Scale |
| −9.920 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | Negative Full-Scale |
Figure 43. Wide BW Low Noise, Low Drift Amplifier

Parasitic input capacitance C1 ≃ (3 pF for LF155, LF156 and LF357 plus any additional layout capacitance) interacts with feedback elements and creates undesirable high frequency pole. To compensate add C2 such that: R2 C2 ≃ R1 C1.
Figure 44. Boosting the LF156 With a Current Amplifier

Figure 45. Decades VCO
R1, R4 matched. Linearity 0.1% over 2 decades.

Figure 46. Isolating Large Capacitive Loads

Figure 47. Low Drift Peak Detector
Figure 48. Noninverting Unity Gain Operation for LF157

Figure 49. Inverting Unity Gain for LF157

Figure 50. High Impedance, Low Drift Instrumentation Amplifier

Figure 51. Fast Sample and Hold

Figure 52. High Accuracy Sample and Hold
Figure 53. High Q Band Pass Filter

Figure 55. VOS Adjustment
Figure 56. Driving Capacitive Loads
Figure 57. LF357 - A Large Power BW Amplifier
For distortion ≤ 1% and a 20 Vp-p VOUT swing, power bandwidth is: 500 kHz.