| 15:8 | MATCH_DATA | R/W | 0x1C | The character to match for buffer release. Normally it is a /R/=/K28.0/-0x1C but with these bits the user can program the value. |
| 7 | MATCH_SPECIFIC | R/W | 1 | Match a specific character to start the JESD buffering when asserted; otherwise the first non-K will start the buffering. |
| 6 | MATCH_CTRL | R/W | 1 | When asserted the match character is a CONTROL character instead of a DATA character. |
| 5 | NO_LANE_SYNC | R/W | 0 | Assert if the TX side does not support lane initialization. This way the RX won’t flag errors in the configuration portion of the ILA. |
| 4:2 | Not Used | R/W | 000 | Not Used |
| 1 |
Reserved |
R/W |
0 |
Reserved |
| 0 | JESD_COMMAALIGN_ENA | R/W | 1 | When asserted the JESD block SERDES comma align signal will be added with the SERDES ALIGN bit(0) to control when to shut off comma alignment. When this bit is deasserted; then the programmed bit(spi_config62(11)) is the only control. |