ZHCSMY8B September 2020 – January 2022 BQ769142
PRODUCTION DATA
Some device pins may not be needed in a particular application. The manner in which each should be terminated in this case is described below.
Pin | Name | Recommendation |
---|---|---|
1–16, 48 | VC0–VC14 | Cell inputs 1, 2, and 14 should always be connected to actual cells, with cells connected between VC1 and VC0, VC2 and VC1, and VC14 and VC13A. VC0 should be connected through a resistor and capacitor on the pcb to pin 17 (VSS). Pins related to unused cells (which may be cell 3–cell 13) can be connected to the cell stack to measure interconnect resistance or provide a Kelvin-connection to actual cells, in which case they should include a series resistor and parallel capacitor, in similar fashion to pins connected to actual cells (see Usage of VC Pins for Cells Versus Interconnect). Another option is to short unused VC pins directly to an adjacent VC pin. All VC pins should be connected to either an adjacent VC pin, an actual cell (through R and C) or stack interconnect resistance (through R and C). |
18, 20 | SRP, SRN | If not used, these pins should be connected to pin 17 (VSS). |
19, 44 | NC | These pins are not connected to silicon. They can be left floating or connected to an adjacent pin or connected to VSS. |
21, 23, 25, 28, 29, 30, 31, 32 | TS1, TS3, ALERT, HDQ, CFETOFF, DFETOFF, DCHG, DDSG | If not used, these pins can be left floating or connected to pin 17 (VSS). Any of these pins (except for TS1 and TS3) may be configured with the internal weak pulldown resistance enabled during operation, although this is not necessary. |
22 | TS2 | If the device is intended to enter SHUTDOWN mode, the TS2 pin should be left floating. If SHUTDOWN mode will not be used in the application, and the TS2 pin will not be used for a thermistor or ADCIN measurement, the TS2 pin can be left floating or connected to pin 17 (VSS). |
33 | RST_SHUT | If not used, this pin should be connected to pin 17 (VSS). |
34, 35 | REG1, REG2 | If not used, these pins can be left floating or connected to pin 17 (VSS). |
36 | REGIN | If not used, this pin should be connected to pin 17 (VSS). |
37 | BREG | If this pin is not used and pin 36 (REGIN) is also not used, both pins should be connected to pin 17 (VSS). If this pin is not used but pin 36 is used (such as driven from an external source), then this pin should be connected to pin 36 (REGIN). |
38 | FUSE | If not used, this pin can be left floating or connected to pin 17 (VSS). |
39 | PDSG | If not used, this pin should be left floating. |
40 | PCHG | If not used, this pin should be left floating. |
41 | LD | If the DSG driver will not be used, this pin can be connected through a series resistor to the PACK+ connector, or can be connected to pin 17 (VSS). |
43 | DSG | If not used, this pin should be left floating. |
45 | CHG | If not used, this pin should be left floating. |
46 | CP1 | If not used, this pin should be connected to pin 47 (BAT). Note: If the charge pump is enabled with
CP1 connected to BAT, the device will consume an additional ≈200
µA. |