ZHCSMY8B September 2020 – January 2022 BQ769142
PRODUCTION DATA
An example circuit layout using the BQ76952 device in a 16-series cell design is described below. The design implements the schematic shown in https://www.ti.com.cn/cn/lit/gpn/bq76952 and uses a 2.75-inch × 3.9-inch 2-layer circuit card assembly, with cell connections on the left edge, and pack connections along the top edge of the board. Wide trace areas are used, reducing voltage drops on the high current paths.
The board layout, which is shown in Figure 18-1 and Figure 18-2, includes spark gaps with the reference designator prefix E. These spark gaps are fabricated with the board and no component is installed.