******************************************************************************
******************************************************************************
**********************  C L O C K   S K E W  F I L E  ************************
******************************************************************************
******************************************************************************
* 
* 
* This is an example skew data file for defining clock skew on
* synchronous/common-clock transfers between a Source device and a Target
* device.
* 
* It's assumed that the Source device has a timing model with DELAY statements
* between output pins relative to a clock input pin (SourceClkPin) and the
* Target device has SETHLD constraints on input pins relative to a clock input
* pin (TargetClkPin). This file defines the clock skew between these pins to
* be used for setup/hold margin calculation during static timing analysis. 
*
* Clock skew is always defined as the worst-case difference between the time
* the clock arrives at the TargetClkPin and the SourceClkPin,
* (E.g., TargetClkPin-SourceClkPin) and should account for all variations in
* the clock distribution system that can add uncertainty or offsets to the
* respective clock pins. There are two types of clock skew, SetupSkew
* and HoldSkew.
* 
* The syntax is: <SourceClkPin>  <TargetClkPin>  <SetupSkew>  <HoldSkew>
*
* Where:
* 
* 1) <SourceClkPin> is the pin on the Source device from which DELAY
* statements on that device's timing model are defined.
*    Note: A device may have more than one SourceClkPin, and separate skew
*          statements will need to be defined for each pin.
* 
* 2) <TargetClkPin> is the pin on the Target device from which SETHLD
* (Setup/Hold) constraints on that devices's timing model are defined with
* respect to.
*    Note: A device may have more than one TargetClkPin, and separate skew
*          statements will need to be defined for each pin.
* 
* -) SourceClkPin and TargetClkPin can be defined in one of five formats with
* precedence shown:  
*        <part_name>/<pinname> 
*        <designator>/<pinname> 
*        <designator>/<part_name>/<pinname> 
*        <reference_designator>.<pinumber>
*        <board_id>/<reference_designator>.<pinumber>
* Note: The format used for SourceClkPin must be the same as
* that used for TargetClkPin
* 
*    a) <part_name> corresponds to the SiAuditor part name defined in the part
*    library
*    
*    b) <pinname> corresponds to the logical pin name for the SourceClkPin or
*    TargetClkPin as it appears in both the IBIS and Timing models.
*    Note: The logical pin names in the IBIS model must match those in
*          the Timing model.
*    
*    c) <designator> corresponds to the name of the graphical I/O buffer in
*    the schematic sheet for the respective Source or Target device.
*    Note: An interface can have multiple sheets, each of which may refer to a
*          designator using a different name. 
*    
*    d) <reference_designator> corresponds to the unique part identifier in
*    the CAD/layout database. (E.g. U21, U55, etc.)
*    
*    e) <board_id> corresponds to the unique board name associated with the
*    CAD/layout database during the Board Extraction and Assignment process.
* 
* 3) <SetupSkew> is defined as the worst-case difference between the earliest
* Target clock and the latest Source clock.
* (E.g., SetupSkew = Min_Target_Clk - Max_Source_Clk)  
* Note: Positive numbers for SetupSkew mean that the clock arrives at the
*       TargetClkPin after it arrives at the SourceClkPin under worst-case
*       conditions. Positive SetupSkew helps setup margin.
* 
* 4) <HoldSkew> is defined as the worst-case difference between the latest
* Target clock and the earliest Source clock.
* (E.g., HoldSkew = Max_Target_Clk - Min_Source_Clk)
* Note: Positive numbers for HoldSkew mean that the clock arrives at the
*       TargetClkPin after it arrives at the SourceClkPin under worst-case
*       conditions. Positive HoldSkew hurts hold margin)
* 
*
******************************************************************************
****************************  E X A M P L E S  *******************************
******************************************************************************
* 
******************************************************************************
* This example shows skew defined using partname/pinname syntax. 
*
* partname/pinname     partname/pinname    SetupSkew (ns)  HoldSkew (ns)   
* sdram/clk            northbridge/clock     -0.4           0.3
* northbridge/clock    sdram/clk             -0.4           0.3
*
******************************************************************************
* This example shows skew defined using designator/partname/pinname syntax. 
*
* designator/partname/pinname  designator/partname/pinname  SetupSkew HoldSkew
* sdram1/sdram/clk              northbridge/northbridge/clock  -0.42     0.32
* northbridge/northbridge/clock sdram1/sdram/clk               -0.42     0.32
* sdram2/sdram/clk              northbridge/northbridge/clock  -0.37     0.27
* northbridge/northbridge/clock sdram2/sdram/clk               -0.37     0.27
*
******************************************************************************
* This example shows skew for post-layout analysis defined using
*  ref_des.pinumber syntax:
*
* ref_des.pinnumber  ref_des.pinnumber  SetupSkew (ns)  HoldSkew (ns)
* U2.B30             U3.23               -0.42           0.32
* U3.23              U2.B30              -0.42           0.32
* U2.B30             U4.23               -0.37           0.27
* U4.23              U2.B30              -0.37           0.27
*
******************************************************************************
*
* This example show clock skew for post-layout defined using
*  board_id/ref_des.pinumber syntax:
*
* board_id/ref_des.pinumber   board_id/ref_des.pinumber SetupSkew HoldSkew
* motherboard/U2.B30          motherboard/U3.23          -0.42     0.32
* motherboard/U3.23           motherboard/U2.B30         -0.42     0.32
*								   
* motherboard/U2.B30          daughtercard/U4.23         -0.37     0.27
* daughtercard/U4.23          motherboard/U2.B30         -0.37     0.27
*
******************************************************************************
* The following are the skews associated with the quickstart project -
*  synchronous interface example in the clock_skew.txt file.
*
* source_designator/clock_pin target_designator/clock_pin  SetupSkew HoldSkew
source/CLOCK_IN               target/CLOCK_IN               -0.50     0.50