无线连接

SimpleLink Wi-Fi CC31xx/CC32xx – 工具与软件

TI 提供多种硬件、开发工具和软件开发套件,包括用于 SimpleLink™ Wi-Fi® 系列的示例应用、驱动程序和 PC 工具

<Section CTA Link - not authored>
<Horizontal Rule is not displayed>
<Section CTA Link - not authored>
<Horizontal Rule is not displayed>

评估套件

CC32xx 无线微控制器 (SoC) 开发套件
LaunchPad & 评估套件 说明 价格
SimpleLink Wi-Fi CC3220SF LaunchPad with QFN-packaged device Evaluation kit used to start your development on the CC3220SF single-chip microcontroller and Wi-Fi solution

Starting at $49.99

Buy now

SimpleLink Wi-Fi CC3220S LaunchPad with QFN-packaged device Evaluation kit used to start your development on the CC3220S single-chip microcontroller and Wi-Fi solution

Starting at $39.99

Buy now

TI SimpleLink Wi-Fi CC3200 LaunchPad kit with QFN-packaged device & LaunchPad kit with certified module Evaluation kit used to start your development on the CC3200 single-chip microcontroller and Wi-Fi solution

Starting at $29.99

Buy now

CC31xx 无线网络处理器开发套件
BoosterPack & 评估套件 说明 价格
SimpleLink Wi-Fi CC3120 wireless network processor BoosterPack plug-in module with QFN-packaged device. Plug-in module for TI LaunchPad kits to add Wi-Fi to your system. Note: The emulation BoosterPack is required to flash the CC3120 and for advanced debugging

Starting at $29.99 

Buy now

SimpleLink Wi-Fi CC3120 BoosterPack + Advanced Emulation BoosterPack for SimpleLink Wi-FI + MSP-EXP432P401R LaunchPad Bundle The SimpleLink Wi-Fi CC3120 wireless network processor BoosterPack plug-in module with QFN-packaged device, Advanced emulation BoosterPack kit, and MSP-EXP432P401R LaunchPad kit. Make for a one-stop evaluation solution

Starting at $55.98

Buy now

SimpleLink Wi-Fi CC3100 wireless network processor BoosterPack with QFN-packaged device or BoosterPack plug-in module with certified module Plug-in module for TI LaunchPad kits to add Wi-Fi to your system. The emulation BoosterPack is required to flash the CC3100 and for advanced debugging

Starting at $19.99 

Buy now

SimpleLink Wi-Fi CC3100 wireless network processor BoosterPack plug-in module + SimpleLink Wi-Fi advanced emulation BoosterPack plug-in module + MSP-EXP430F5529LP LaunchPad kit The SimpleLink Wi-Fi CC3100 wireless network processor BoosterPack plug-in module, advanced emulation BoosterPack kit, and MSP430F5529 LaunchPad kit make for a for a one-stop evaluation solution

$53.99

Buy now

软件

常见软件 说明
SimpleLink Wi-Fi starter pro The SimpleLink Wi-Fi Starter Pro mobile App is a new mobile application for SimpleLink provisioning.
Wi-Fi provisioning Wi-Fi provisioning is the process of connecting a new Wi-Fi device (station) to a Wi-Fi network (access point). This process involves loading the station with the network name (SSID) and its security credentials. TI’s SimpleLink Wi-Fi family offers the most flexibility for provisioning options including Access Point Mode, WPS, TI’s SmartConfig technology and others.
无线 MCU 器件 说明
CC3220 Software Development kit and Firmware CC3220 The Texas Instruments royalty-free CC3220 Embedded Wi-Fi foundation software development kit (SDK) is a complete software platform for developing Wi-Fi applications. This SDK contains drivers for the CC3220 programmable MCU, sample applications, peripheral drivers, and documentation needed to use the CC3220 solutions.
All sample applications are supported on the integrated Cortex®-M4 with Code Composer Studio IDE and on RTOS. Some applications support IAR, GCC, TI RTOS and free RTOS
CC3200 software development kit and firmware CC3200 The CC3200 SDK contains drivers for the integrated programmable MCU, 40+ sample applications for Wi-Fi features, internet applications, and peripheral functions with associated documentation needed to use the solution. This SDK can be used with the SimpleLink Wi-Fi CC3200 wireless MCU evaluation boards.
All sample applications are supported on the integrated Cortex®-M4 with Code Composer Studio IDE and on RTOS. Some applications support IAR, GCC, TI RTOS and free RTOS
Programmers Guide CC3220 A programmer’s guide for for SimpleLink Wi-Fi CC3220, a single-chip wireless MCU
Programmers Guide CC3120/CC3220 A programmer’s guide for SimpleLink Wi-Fi CC3120/CC3220 & Internet of Things processor
Programmers Guide CC3100/CC3200 A programmer’s guide for SimpleLink Wi-Fi CC3100/CC3200 & Internet of Things processor
无线网络处理器 器件 说明
CC3120 software development kit and firmware CC3120 The CC3120 SDK contains drivers and sample applications for the CC3120 Wireless Network Processor. The SDK can be used with TI’s MSP-432LaunchPad kit or SimpleLink Studio, a PC tool that allows MCU development with CC3120. You can also use the SDK as example code for any platform
All sample applications are supported via Code Composer Studio™ integrated development environment (IDE) and on RTOS. Some applications are supported via IAR.
CC3100 software development kit and firmware CC3100 The CC3100 SDK contains drivers, many sample applications for Wi-Fi features and Internet and documentation needed to use the CC3100 Internet-on-a-chip™ solution. This SDK can be used with TI’s MSP-EXP430F5529LP LaunchPad kit or SimpleLink Studio, a PC tool that allows MCU development with CC3100. You can also use the SDK as example code for any platform.
All sample applications are supported via Code Composer Studio™ integrated development environment (IDE) and on RTOS. Some applications are supported via IAR.

开发工具

常见工具 器件 说明
Uniflash tool CC32xx & CC31xx A standalone tool used to program the external flash memory
Radio testing tool

CC32xx &

CC31xx

Send commands to configure Wi-Fi in different test operation modes (receive and transmit). This tool is required for regulatory certification
集成开发环境 (IDE) 器件 说明
Code Composer Studio™ IDE CC32xx & CC31xx Code Composer Studio IDE comprises a suite of tools used to develop and debug embedded applications.
IAR embedded workbench CC32xx & CC31xx IAR Embedded Workbench Kickstart for MSP MCUs is a complete debugger and C/C++ compiler toolchain for building and debugging embedded applications based on MSP430™ and MSP432 microcontrollers.
Open source GCC for MSP MCUs CC32xx & CC31xx TI has partnered with Red Hat to offer a new and fully supported open source compiler as the successor to the community driven MSPGCC. This free GCC 4.9 compiler supports all MSP430 devices and has no code size limit.
无线网络处理器 器件 说明
SimpleLink Studio for CC31xx CC31xx A PC based tool used to mimic MCU control of the CC31xx devices
无线 MCU 器件 说明
Pin-mux utility CC32xx Choose peripheral combinations that meet your system needs