电机驱动和控制解决方案

为 AC 感应电机 (ACIM)、刷式直流电机、无刷直流电机 (BLDC)、永久磁性同步电机和步进电机等各类电机,寻找合适的模拟和数字产品、软件和支持,以精确控制位置、速度和扭矩


 

Success Stories: Supporting youth robotics competition with TI expertise and components

Texas Instruments is proud to be a FIRST Crown Supplier for the 2011 competition season; the highest contribution level a supplier can receive. TI's primary contribution are the Stellaris MDL-BDC "Jaguar" and MDL-BDC24 "Black Jaguar" Speed Controllers provided to FIRST for inclusion in FIRST's official FRC Kit of Parts distributed to more than 2,000 competing FRC teams around the globe – that's over 10,000 FRC mentors (engineering professionals / TI customers), 50,000 high school students (young engineers), and countless parents and volunteers that will actively use a Jaguar – thus TI – for the FRC build season and competition starting January 8, 2011.

FIRST is a not-for-profit organization founded in 1989 by Dean Kamen to inspire young people's interest and participation in science and technology. The focal FIRST program is FIRST Robotics Competition (a.k.a. "FRC"); a high school robotics competition where teams are provided an official FIRST Kit of Parts (about $6000 worth of equipment), game rules, and then 6 weeks to conceptualize, design, build, and postmark their competing robot to their preferred initial FRC Regional competition. There are approximately 40 regional competitions around the world spanning over 6 weeks, which lead up to a Championships Event held in the Edward Jones Dome in St. Louis, MO on April 27-30, 2011. Learn more about this year's FRC game: LOGO MOTION™.

Based on Texas Instruments' powerful Stellaris 32-bit microcontrollers, the Stellaris MDL-BDC "Jaguar" and MDL-BDC24 "Black Jaguar" modules are intelligent, variable speed control and power drive for 12V and 24V brushed DC motors – with integrated features that allow the ability to easily control and entire network of Jaguars over CAN. While the products are designed for robust, real-time control and connectivity of high voltage/high-power motion control in a potentially "high-impact" and "noisy" robotics environment, each module is designed for simplicity and ease-of-use such that they are not intimidating for high school student to use in competition.

The MDL-BDC24 "Black Jaguar" is available and legal for use in the FRC 2011 competition, called LOGO MOTION™. Since TI is renowned for high precision analog solutions, the MDL-BDC24 incorporates several high-quality analog components from Texas Instruments, including the SN65HVD1050 CAN Transceiver, MAX3221 RS232 Line Driver/Receiver, TPS54040 Swift DC/DC converter, TPS73633 Voltage Regulator, and INA193 Current Shunt Monitor.  At the heart of the MDL-BDC24 is TI's Stellaris LM3S2616 ARM Cortex-M3-based MCU.

MDL-BDC24 "Black Jaguar"

So how does TI's MDL-BDC24 "Black Jaguar" help teams succeed?

MDL-BDC Jaguar was inspired by FIRST Robotics Team Mentors (working at TI) that envisioned a superior speed controller based on the advanced microcontroller technology for motion control. While envisioning this superior speed controller:

The MDL-BDC24 ships as a ready-to-run, yet customizable, module with the following features:

  • Quiet control of brushed DC motors
    • 15 kHz Hbridge frequency
  • Three options for open-loop voltage control
    • Industry-standard R-C servo type (PWM) interface
    • Controller Area Network (CAN) interface
    • RS232 serial interface
  • Two options for closed-loop, speed, position, or current control
    • Controller Area Network (CAN) interface
    • RS232 serial interface
  • CAN communication
    • Full configurability of module options
    • Real-time monitoring of current, voltage, speed, and other parameters
    • Load firmware over RS232/CAN
  • RS232 serial communication
    • Bridges an RS232-enabled device to the CAN
    • Directly interfaces to a PC serial port or National Instruments cRIO
  • Limit switch inputs for forward and reverse directions
  • Firmware features
    • Full configurability of closed-loop module parameters
    • Real-time monitoring of sensor data including motor current, encoder position or speed, and limit switch state
  • Status LED indicates run, direction, and fault conditions
  • Motor brake/coast selector
  • Quadrature encoder input (QEI) and analog input
  • Color-coded screw terminals for all power wiring