CC1350STK
Simplelink CC1350 SensorTag 蓝牙和低于 1GHz 的远距离无线开发套件
CC1350STK
概述
CC1350 SensorTag 借助单芯片 Bluetooth™ Smart® 无线电和低于 1GHz 的无线电,扩展了 SensorTag 生态系统,实现了轻松手机集成与远距离连接的完美组合,在单个芯片上配有 32 位 ARM® Cortex®-M3 处理器,使用单个纽扣电池可运行数年。
CC1350 器件是一款面向低功耗、远距离无线应用的无线 MCU。CC1310 器件包含一个作为主处理器以 48MHz 运行的 32 位 ARM® Cortex®-M3 处理器,还包含丰富的外设功能集,其中包括一个独特的超低功耗传感器控制器。此传感器控制器非常适合连接外部传感器,还适用于在系统其余部分处于睡眠模式的情况下自主收集模拟和数字数据。
CC1350 SensorTag 可借助蓝牙实现与智能手机和平板电脑的直接连接,与 2Km 的范围相结合,适用于低于 1GHz 的无线电接口。
特性
- 具有蓝牙和低于 1GHz 无线电的 SensorTag,适用于带有集成型 PCB 迹线天线的无线应用
- 包括 10 个低功耗 MEMS 感应器,适用于感应运动、温度、湿度、压力、光、磁场和声音
- 与 Debug DevPack 兼容,适用于在 CCS Cloud 和 CCS 桌面中进行即时代码开发
- 受 SensorTag 应用支持
- 1 x CC1350 SensorTag
立即订购并开发
CC1350STKEU — Simplelink CC1350 SensorTag 蓝牙和低于 1GHz 的远程无线开发套件
CC1350STKUS — Simplelink CC1350 SensorTag 蓝牙和低于 1GHz 的远距离无线开发套件
FLASH-PROGRAMMER-2 — SmartRF 闪存编程器 v2
Zip file with Windows Installer and SW Manifest
产品
低功耗 2.4GHz 产品
Sub-1GHz 无线 MCU
其他无线产品
汽车类无线连接产品
硬件开发
文档
Compressed source file archive
发布信息
SmartRF Flash Programmer 2 can be used to program the flash memory in Texas Instruments ARM based low-power RF wireless MCUs over the debug and serial interfaces. The flash programmer includes both a graphical user interface and a command line interface.
最新信息
- Support for the CC2640R2L added.
- Updated emupack to version 9.2.0.00002.
SMARTRF-STUDIO-7 — SmartRF Studio
产品
MSP430 微控制器
低功耗 2.4GHz 产品
Sub-1GHz 无线 MCU
Sub-1GHz 收发器
其他无线产品
汽车类无线连接产品
硬件开发
开发套件
评估板
文档
SmartRF Studio 7 in Cloud TI Resource Explorer
Compressed source file archive
发布信息
SmartRF™ Studio is a Windows application that can be used to evaluate and configure Low Power RF devices from Texas Instruments. The application helps designers of RF systems to easily evaluate the radio at an early stage in the design process. It is especially useful for generation of configuration register values and commands, and for practical testing and debugging of the RF system. SmartRF Studio can be used either as a standalone application or together with applicable evaluation boards or debug probes for the RF device.
最新信息
- Updated RF PHY settings for the CC13x4/CC26x4 devices
- Various improvements and bug-fixes
SIMPLELINK-CC13X0-SDK — SimpleLink™ CC13x0 软件开发套件
产品
Sub-1GHz 无线 MCU
硬件开发
发布信息
The SimpleLink™ CC13x0 Software Development Kit (SDK) is part of the Texas Instruments SimpleLink family of wireless microcontrollers (MCUs), offering a single development environment that delivers flexible hardware, software and tool options for customers developing wired and wireless applications. For more information about the SimpleLink MCU platform, visit www.ti.com/simplelink.
SimpleLink™ CC13x0 Software Development Kit is a set of software development tools that enables engineers to develop software applications on the SimpleLink™ CC13x0 ULP devices. This powerful software toolkit provides a cohesive and consistent software experience for all SimpleLink™ CC13x0 users by packaging essential software components such as TI RTOS, peripheral drivers, TI 15.4-Stack, Bluetooth Low Energy, and RF-Proprietary examples in one easy-to-use software package along with exhaustive documentation.
This is version 4.20.02.07 of the SimpleLink CC13x0 SDK.
最新信息
- The ECDH and ECDSA driver has been updated with new validation options. This driver will now validate public key, random string, signature and private key before driver operations.
- Bugfix for the TI 15.4-Stack
- SimpleLink platform level changes are available in SimpleLink Core SDK Release Notes
- SDK Change Log provides a list of all SDK component changes
- Please refer to the Document Overview for the individual release notes and details for starting development with each SDK component
SENSOR-CONTROLLER-STUDIO — Sensor Controller Studio
Installer executable
Compressed archive
产品
低功耗 2.4GHz 产品
Sub-1GHz 无线 MCU
其他无线产品
汽车类无线连接产品
硬件开发
开发套件
文档
HTML document
Compressed source file archive
发布信息
Sensor Controller Studio is used to write, test and debug code for the CC26xx/CC13xx Sensor Controller, allowing for ultra-low power application design.
The tool generates a Sensor Controller Interface driver, which is a set of C source files to be compiled into the System CPU (ARM Cortex-M3/M4) application. These source files contain the Sensor Controller firmware image and associated definitions, and generic functions that allow the System CPU application to control the Sensor Controller and exchange data.
The Sensor Controller is a small CPU core that is highly optimized for low power consumption and efficient peripheral operation. The Sensor Controller is located in the CC26xx/CC13xx auxiliary (AUX) power/clock domain, and can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power state. Such tasks include but are not limited to:
- Analog sensor polling, using ADC or comparator
- Digital sensor polling, using SPI, I2C or other protocols
- Capacitive sensing, using current source, comparator and time-to-digital converter (TDC)
- Waveform generation, for example for LCDs
The Sensor Controller is user programmable, using a simple programming language with syntax similar to C. This allows for sensor polling and other tasks to be specified as sequential algorithms, rather than static configuration of complex peripheral modules, timers, DMA, register programmable state machines, event routing and so on. The main advantages are:
- Flexibility
- Dynamic reuse of hardware resources
- Ability to perform simple data processing without need for dedicated hardware
- Observability and debugging options
最新信息
- Added support for new devices: CC2672R3, CC2672P3, CC2662R-Q1, CC2652PSIP and CC2652P7.
- Added example support for new SDKs, using TI-RTOS 7 and GPIO driver for the latest CC13x2/CC26x2 SDK.
- Minor improvements.
- Bug-fixes.
TI-15-4-STACK-GATEWAY-LINUX-SDK — TI 15-4-Stack 网关 Linux 软件开发套件
Link to TI 15.4-Stack Gateway Linux installer
产品
Sub-1GHz 无线 MCU
硬件开发
文档
TI 15.4-Stack Linux Gateway User Guide
最新信息
- Maintenance release
发布信息
- Developers targeting products based on TI 15.4-Stack have two architecture choices for their product development.
- First option is to have entire TI 15.4-Stack application and stack run within the SimpleLink CC13x0/CC13x2 MCU (as an embedded application) while the second option is to have the application running on a host (running Linux OS, etc) interfacing to the SimpleLink ULP CC13x0/CC13x2 MCU running the MAC Co-Processor Application. This TI 15.4-Stack Linux SDK provides example Linux host applications, tools, documentation that allow to develop products using the architecture option two using a Linux host interfacing with the CC13x0/CC13x2 running MAC CoProcessor as described above.
设计文件
技术文档
类型 | 标题 | 下载最新的英文版本 | 日期 | |||
---|---|---|---|---|---|---|
* | 更多文献资料 | CC1350 SensorTag Quick Start Guide (Rev. A) | 2017年 3月 29日 | |||
证书 | CC1350STKUS EU Declaration of Conformity (DoC) | 2019年 1月 2日 | ||||
证书 | CC1350STKEU EC Declaration of Conformity (DoC) (Rev. A) | 2019年 1月 2日 | ||||
用户指南 | CC1350 LaunchPad Getting Started Guide (Rev. B) | 2018年 6月 20日 |