MSP430 并行端口调试接口
MSP-FET430PIF
该产品可持续生产,以支持现有客户。

描述/特性

技术文档

支持与培训

订购选项


主要文档
Download - PDF Icon

描述

The MSP-FET430PIF is a Parallel Port interface (does not include target board) that is used to program and debug MSP430 FET tools and test boards through the JTAG interface. This interface is included in our FET tools, but sold without the development board. This interface uses a Parallel PC Port to communicate to the Debugger Software (IAR Kickstart software included) running on the PC. The interface uses the standard 14 pin header to communicate to the MSP430 device using the standard JTAG protocol.

The flash memory can be erased and programmed in seconds with only a few keystrokes, and since the MSP430 flash is extremely low power, no external power supply is required. The tool has an integrated software environment and connects directly to the PC which greatly simplifies the set-up and use of the tool. The flash development tool supports development with all MSP430 flash parts.

特性
  • MSP430 debugging interface to connect a MSP430-Flash-device to a Parallel port on a PC
  • Supports JTAG debug protocol (NO support for Spy-Bi-Wire (2-wire JTAG) debug protocol, Spy-Bi-Wire (2-wire JTAG) is supported by MSP-FET430UIF)
  • Parallel Port cable and a 14-conductor target cable
  • Full documentation on CD ROM
  • Integrated IAR Kickstart user interface which includes:
    • Assembler
    • Linker
    • Limulator
    • Source-level debugger
    • Limited C-compiler
  • Technical specifications:
    • Backwardly compatable with existing FET tool boards.

包含项目
  • One READ ME FIRST document
  • One MSP430 CD-ROM
  • One 14-conductor cable
  • One 25-conductor cable
  • One MSP-FET430PIF interface module

TI's Standard Terms and Conditions for Evaluation Modules apply.

技术文档
更多文献资料 (1)
标题 日期 类型
MSP-EXP430XXXX Software Examples 2015年 5月 6日
用户指南 (8)
标题 类型 大小 (KB) 日期 下载最新英文版本
PDF 1039 2013年 11月 15日 下载最新的英文版本 (Rev.AR)
PDF 7200 2012年 12月 30日 下载最新的英文版本 (Rev.AE)
PDF 4524 2019年 2月 27日
PDF 8156 2018年 11月 1日
PDF 1701 2018年 5月 11日
PDF 995 2018年 5月 11日
PDF 1662 2017年 11月 13日
PDF 829 2017年 11月 13日
相关产品

软件 (1)


开发工具 (2)

名称 器件型号 工具类型
MSP430 USB 调试接口  MSP-FET430UIF  Debug Probes/Analyzers 
TI Code Composer Essentials 评估 - 免费 16KB IDE  MSP-CCE430  软件开发工具、IDE、编译器 

支持与培训

搜索我们广泛的在线知识库,可全天候获得数百万个技术问题和答案。

从 TI 专家处搜索答案

由TI和其社区用户提供的内容仅符合当时状况,不视为TI的标准说明。
请详见网站使用条款

如果您对质量、包装或订购 TI 产品有疑问,请访问我们的支持页面

技术文章