SimpleLink™ 低功耗 Bluetooth® CC2640R2F 无线 MCU LaunchPad™ 开发套件
LAUNCHXL-CC2640R2
此产品已上市,且可供购买。 可提供某些产品的较新替代品。

描述/特性

技术文档

支持与培训

订购选项


Important Note

Getting started on CC2640R2F is simple! Read our blog to learn how.

View all related products

主要文档
Download - PDF Icon

描述

To get started developing with this LaunchPad:
Step 1: Buy the CC2640R2 LaunchPad
Step 2: Download the CC2640R2 SDK
Step 3: Take the CC2640R2 SimpleLink Academy trainings

The CC2640R2F device has the first fully qualified Bluetooth 5 protocol stack for single-mode Bluetooth low energy applications supporting high speed mode.  CC2640R2F is part of the SimpleLink™ microcontroller (MCU) platform which consists of Wi-Fi®, Bluetooth® low energy, Sub-1 GHz and host MCUs, which all share a common, easy-to-use development environment with a single core software development kit (SDK) and rich tool set. A one-time integration of the SimpleLink platform enables you to add any combination of the portfolio’s devices into your design, allowing 100 percent code reuse when your design requirements change. For more information, visit www.ti.com/simplelink

The CC2640R2 LaunchPad kit brings easy Bluetooth® low energy (BLE) connection to the LaunchPad ecosystem with the SimpleLink ultra-low power CC26xx family of devices. Compared to the CC2650 LaunchPad this LaunchPad has:

  • More free flash memory for the user application in the CC2640R2F wireless MCU
  • Out of the box support for Bluetooth 5 high speed mode and Bluetooth 4.2 specification
  • Demo Bluetooth 5 coded physical layers (PHY) for long range mode testing (Bluetooth 5 long range mode stack support will be enabled with future software updates)

The CC2640R2F wireless MCU contains a 32-bit ARM® Cortex®-M3 processor that runs at 48 MHz as the main microcontroller and a rich peripheral feature set that includes a unique ultra-low power sensor controller. This sensor controller was created for interfacing external sensors and for collecting analog and digital data autonomously while the rest of the system is in sleep mode.

The CC2640R2 LaunchPad kit is optimized for BLE applications with more flash memory available. It supports programming and debugging from Code Composer Studio™ and IAR Embedded Workbench® integrated development environments (IDEs).

Get started by downloading the TI BLE Stack and start with Project 0. This is a fully functional Bluetooth low energy peripheral application allowing control of the LaunchPad kit’s LEDs from the TI SimpleLink SensorTag kit iOS app or any compatible device supporting Bluetooth low energy connectivity. The project also demonstrates the flexibility of the TI RTOS and utilizes the LaunchPad kit’s onboard USB serial port to display diagnostic information about the Bluetooth low energy connection.

Ready to take your application development to the next level? Save time and production cost by quickly prototyping your system with the LaunchPad kit I/O connectors that allow for quick interfacing to a variety of evaluation modules (EVMs) and BoosterPack™ plug-in modules. Develop your Internet of Things (IoT) software application on the CC2640R2 LaunchPad kit using the TI BLE-Stack™ Software Development Kit (SDK) featuring royalty-free Bluetooth 5 and 4.2 certified software stacks. A Bluetooth low energy user’s guide for the LaunchPad kit is available on TI Resource Explorer  with instructions for building the most popular sample applications on the CC2640R2 LaunchPad kit.

特性
  • Support for new Bluetooth 5 2Mbps high speed mode
  • Connect your LaunchPad to the cloud with Bluetooth low energy on your Smartphone
  • Access all I/O signals with the BoosterPack connectors
  • Upgrade the LaunchPad firmware over-the-air from the SimpleLink Starter app

包含项目

  • LaunchPad board
  • Micro USB cable
  • Quick Start Guide
  • SZZC019 - Kit Stuffer

立即订购
器件型号 从德州仪器 (TI) 或第三方购买 通知我 结帐选项 状态

LAUNCHXL-CC2640R2:
CC2640R2 LaunchPad

$29.00(USD)


价格可能会不同



ACTIVE

SIMPLELINK-CC2640R2-SDK :
SimpleLink CC2640R2 Software Development Kit

免费



无此商品 ACTIVE

SIMPLELINK-ETHERNET-BLE :
SimpleLink™ MSP432E4 Ethernet LaunchPad™ + CC2640R2F LaunchPad™ Bundle



无此商品 ACTIVE

应遵守 TI 的评估模块标准条款与条件

技术文档
数据表 (1)
标题 类型 大小 (KB) 日期 下载最新英文版本
PDF 4161 2017年 1月 13日
应用手册 (1)
标题 类型 大小 (KB) 日期 下载最新英文版本
PDF 5355 2019年 1月 9日
白皮书 (5)
标题 类型 大小 (KB) 日期 下载最新英文版本
PDF 2274 2018年 1月 10日
PDF 873 2017年 10月 16日
PDF 1929 2017年 9月 25日
PDF 2974 2017年 7月 19日
PDF 728 2017年 5月 11日
设计文件 (1)
标题 类型 大小 (KB) 日期 下载最新英文版本
ZIP 5459 2016年 12月 9日
更多文献资料 (5)
标题 类型 大小 (KB) 日期 下载最新英文版本
PDF 201 2019年 6月 17日
PDF 400 2019年 2月 6日
PDF 379 2019年 1月 2日
PDF 141 2018年 11月 5日
PDF 395 2017年 9月 18日
相关产品

开发工具 (3)

名称 器件型号 工具类型
SmartRF Studio Download  SMARTRFTM-STUDIO  计算工具 
适用于无线连接的 Code Composer Studio (CCS) 集成开发环境 (IDE)  CCSTUDIO-WCS  软件开发工具、IDE、编译器 
SmartRF 闪存编程器  FLASH-PROGRAMMER  闪存编程工具 

TI 器件 (16)

器件型号 名称 产品系列
CC2640R2F  SimpleLink 低功耗 Bluetooth® 无线 MCU  SimpleLink 解决方案 
CC2640R2F-Q1  符合汽车标准的 SimpleLink 低功耗 Bluetooth® 无线 MCU  SimpleLink 解决方案 
MSP432E401Y  SimpleLink™ 以太网微控制器  SimpleLink MCU 
MSP432E411Y  SimpleLink 以太网微控制器  SimpleLink MCU 
MSP432P4011  具有精密 ADC、2MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P4011T  具有精密 ADC、2MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P401V  具有精密 ADC、512KB 闪存和 128KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P401VT  具有精密 ADC、512KB 闪存和 128KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P401Y  具有精密 ADC、1MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P401YT  具有精密 ADC、1MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P4111  具有精密 ADC、2MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P4111T  具有精密 ADC、2MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P411V  具有精密 ADC、512KB 闪存和 128KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P411VT  具有精密 ADC、512KB 闪存和 128KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P411Y  具有精密 ADC、1MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 
MSP432P411YT  具有精密 ADC、1MB 闪存和 256KB RAM 的 SimpleLink 超低功耗 32位 Arm Cortex-M4F MCU  SimpleLink MCU 

支持与培训

搜索我们广泛的在线知识库,可全天候获得数百万个技术问题和答案。

从 TI 专家处搜索答案

由TI和其社区用户提供的内容仅符合当时状况,不视为TI的标准说明。
请详见网站使用条款

如果您对质量、包装或订购 TI 产品有疑问,请访问我们的支持页面

技术文章