ZHCSGQ5 September 2017 TUSB215-Q1
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The primary purpose of the TUSB215-Q1 is to re-store the signal integrity of a USB High Speed channel up to the USB connector. The loss in signal quality stems from reduced channel bandwidth due to high loss PCB trace and other components that contribute a capacitive load. This can cause the channel to fail the USB near end eye mask. Proper use of the TUSB215-Q1 can help to pass this eye mask. Additionally the DC Boost helps overcoming DC losses from cables and traces.
A secondary purpose is to use the CD pin of the TUSB215-Q1 to control other blocks on the customer platform if so desired. The TUSB215-Q1 also provides CDP controller function.
A typical application is shown in Figure 6. In this setup, D2P and D2M face the USB connector while D1P and D1M face the USB host or hub. If desired, the orientation may be reversed [that is, D2 faces transceiver and D1 faces connector].
For this design example, use the parameters shown in the table below.
PARAMETER | VALUE | |||
---|---|---|---|---|
VCC (4.4 V to 5.5 V) | 5 V | |||
I2C support required in system (Yes/No) | No | |||
AC Boost | REQ | Level | AC Boost Level 2: REQ = 3.83 k |
|
0-Ω | 0 | |||
1.69 k ±1% | 1 | |||
3.83 k ± 1% | 2 | |||
DNI | 3 | |||
DC Boost | RDC1 | RDC2 | Level | Mid DC Level: RDC1 = DNI RDC2 = DNI |
22 kΩ - 47 kΩ | Do Not Install (DNI) | 40 mV Low DC boost | ||
DNI | DNI | 60 mV Mid DC boost | ||
47 kΩ | 24 kΩ | 80 mV High DC boost |
TUSB215-Q1 requires a valid reset signal as described in the power supply recommendations section. The capacitor at RSTN pin is not required if a microcontroller drives the RSTN pin according to recommendations.
VREG pin is the internal LDO output that requires a 0.1-μF external capacitor to GND to stabilize the core.
The ideal AC boost setting is dependent upon the signal chain loss characteristics of the target platform. The general recommendation is to start with AC boost level 0, and then increment to AC boost level 1, etc. if permissible. Same applies to the DC Boost setting where it is recommended to plan for the required pads or connections to change boost settings, but to start with DC boost level 1.
In order for the TUSB215-Q1 to recognize any change to the AC and DC Boost settings, the RSTN pin must be toggled. This is because the configuration is latched on power up and the inputs are ignored thereafter.
NOTE
The TUSB215-Q1 compensates for DC attenuation in the signal path according to the configuration of the DC_BOOST pin. This pin is not 5V tolerant and therefore when selecting the highest DC boost level, the voltage level at DC_BOOST pin must be less than 3.6V.
Placement of the device is also dependent on the application goal. Table 4 summarizes our recommendations.
PLATFORM GOAL | SUGGESTED DEVICE PLACEMENT |
---|---|
Pass USB Near End Mask | Close to measurement point |
Pass USB Far End Eye Mask | Close to USB PHY |
Cascade multiple devices to improve device enumeration | Midway between each USB interconnect |
NOTE
USB-IF certification tests for High Speed eye masks require the mandated use of the USB-IF developed test fixtures. These test fixtures do not require the use of oscilloscope probes. Instead they use SMA cables. More information can be found at the USB-IF Compliance Updates Page. It is located under the ‘Electricals’ section, ID 86 dated March 2013.
The following procedure must be followed before using any oscilloscope compliance software to construct a USB High Speed Eye Mask: