微控制器 (MCU)

设计支持

入门

选择工具

培训

开发者网络

大学

 153 次查看

Digital filtering is an integral part of many digital signal processing algorithms. Digital filters are characterized as either recursive [infinite impulse response (IIR)] or non-recursive [finite impulse response (FIR)] filters. IIR filters require a lower order for the same set of specifications compared to FIR filters, while FIR filters provide a linear phase property. However, IIR filters, if not designed properly, tend to be unstable and use coefficients that are difficult to implement. This application report describes the design of a certain type of IIR digital filter with excellent stability properties, known as a Lattice Wave Digital Filter (LWDF), given a set of analog filter specifications. An elementary knowledge of filters is sufficient to understand the design of LWDF as discussed in this report. The complete design of the basic filters (low-pass, high-pass, and band-pass) is given with examples. The code provided with this application report implements these LWDFs on the MSP430 CPU.

相关文件: