ZHCU734A January   2017  – March 2020

 

  1.   修订历史记录

Software Setup

  1. Open CCS (version 9.3 or newer). Maximize CCS to fill the screen. Close the welcome screen if it opens up.
  2. On the menu bar click Project >Import CCS Project. Below the root directory, navigate to and select ..\C2000Ware_DigitalPower_SDK_X_XX_XX_XX\solutions\tidm_1001\f28002x\llc directory. Make sure that below the Projects tab, 2PH_IL_LLC_F28002x is selected. Click Finish.
  3. 2PH_IL_LLC_F28002x project should now appear in the CCS Project Explorer window. This project will invoke all the necessary tools (compiler, assembler, and linker) to build the project. A project contains all the files and build options required to develop an executable output file (.out), which can be run on the MCU hardware.
  4. In the project window on the left, click the arrow sign to the left of the project name.The project window will look like Figure 22.
  5. TIDM-1001 Project Window.pngFigure 22. Project Window
  6. If not already open, double click the main.sysconfig file name in the project window.
  7. Under Project Options select Open Loop as shown in Figure 23. Save main.syscfg file.
TIDM-1001 Build one powerSUITE GUI.pngFigure 23. Lab One: main.syscfg