TIDUCJ0G November   2016  – April 2020

 

  1.   Revision History

System configuration

Figure 49. Vienna PFC and Ethernet Configuration TIDM-1000 tidm-1000-ethernet-ipc-pfc.gif

There are two data flows in this test as shown in Figure 49. In the parameter monitoring flow, the three phase current, voltage, and power factors are monitored and shown in HTTP GUI page. In the control command flow, the output voltage reference and command signal (Start PFC --cleartrip) can be set in the GUI page and control the Vienna rectifier.