TIDUCJ0G November   2016  – April 2020

 

  1.   Revision History

PWM Modulation

Figure 3 shows a simplified, single-phase diagram of the Vienna rectifier. To control this rectifier, the duty cycle is controlled such that it regulates the voltage vxiNdirectly. That is, if the software variable Duty is set to 1, it makes vxiN the largest voltage possible by never turning on Q1 and Q2 switches and letting the inductor connect to the DC bus though the bridge diode. Similarly when Duty is set to 0, PWM is modulated such that Q1 and Q2 always conduct making vxiN connect to the midpoint of the DC bus (which is zero), which makes it the lowest possible voltage for the switching cycle.

Figure 3. Single Phase Diagram of Vienna RectifierTIDM-1000 SinglePhaseViennaDiagram.gif

Figure 4 shows the detailed PWM configuration.

Figure 4. Vienna Rectifier Detailed PWM Modulation SchemeTIDM-1000 ViennaPWMWaveform-02.gif