10.5.7 Read EEPROM
The contents of the EEPROM can be read out, one word at a time, starting with that of the requested address. The following details the programming sequence for an EEPROM read by address:
- Write the most significant 9th bit of the EEPROM address in R139.0 and write the least significant 8 bits of the EEPROM address in R140.
- The EEPROM data located at the address specified in the step above can be obtained by reading R141 in the same I2C transaction. Any additional access that is part of the same transaction will cause the EEPROM address to be incremented and a read will take place of the next EEPROM address. Access to EEPROM will terminate at the end of current I2C transaction.
NOTE
It is possible to increment EEPROM address incorrectly when 2 successive accesses are made to R140.