ZHCSA85F August 2012 – February 2019 DLPC410
PRODUCTION DATA.
The Reset 2 Blocks (RST2BLK) signal helps to signify a multiple block operation is requested by the user, where, depending on the state of RST2BLK, either two blocks or 4 blocks will be Reset together. The specific blocks to be Reset will then be determined by the Block Mode and Block Address. This signal should be setup synchronously with the start of a row cycle.
NOTE
RST2BLK needs to be kept low during initialization for proper setup of the system.