ZHCSDP2B May 2015 – June 2017
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
It is important to pay special attention to the PCB layout. The following provides some guidelines:
The bq24080-Q1 and bq24081-Q1 are packaged in a thermally enhanced MLP package. The package includes a thermal pad to provide an effective thermal contact between the device and the printed-circuit board (PCB). Full PCB design guidelines for this package are provided in the application report entitled, QFN/SON PCB Attachment (TI Literature Number SLUA271).
The most common measure of package thermal performance is thermal impedance (RθJA) measured (or modeled) from the device junction to the air surrounding the package surface (ambient). The mathematical expression for RθJA is:
Where:
Factors that can greatly influence the measurement and calculation of RθJA include:
The device power dissipation, P, is a function of the charge rate and the voltage drop across the internal Power FET. It can be calculated from the following equation:
Due to the charge profile of Li-xx batteries, the maximum power dissipation is typically seen at the beginning of the charge cycle when the battery voltage is at its lowest. See Figure 6.